Herhangi bir sorunuz mu var? Materyale mi ihtiyacınız var? Güncel basın bilgileri ve baskıya hazır fotoğraf materyallerini buradan ücretsiz yükleyebilirsiniz. Aramanız, e-posta veya faks göndermenizden memnuniyet duyarız! |
|
Basın irtibatMedya dağıtım listemize eklenmek istiyor musunuz? |
Cables for drive technology found, ordered and connectorised quickly at igus3.1.2019
If the user is looking for a drive cable, then igus, with its portfolio of more than 1,350 cables, always has the optimum solution for the respective application at the most cost-effective price. The motion cable specialist has been developing cables specifically for use in the energy chain for over 30 years and testing them in the largest laboratory for moving applications in the industry. With over two billion test cycles and more than 1.4 million electrical tests per year, igus is the number one for moving cables in energy chains. The new website
www.igus.eu/drive now provides a new gateway to the diverse world of igus cables. From cables sold by the metre and the harnessed, ready-to-connect drive cable with connector up to the special cable in the desired length. The customer has a wide choice. The "Drive" website offers the user a comprehensive overview of the drive technology, the igus test laboratory and the in-house harnessing of cables. In addition, the user has the option to order free samples or directly order the appropriate cable that he wants from the shop. |